get a specific Uboot version for the LX2160A-RDB-B (rev2)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

get a specific Uboot version for the LX2160A-RDB-B (rev2)

2,016 Views
Thierry_LOUSSOT
Contributor II

Hi

I am working on the LX2160A-RDB-B (shematic C) and I have issue to start my VxWorks system loaded from tftp

From LX2160ARDB – How to update composite firmware in FlexSPI NOR Flash and SD/eMMC card using an SD card...

all is describe from this link to flash the xspi

https://www.nxp.com/lgfiles/sdk/lsdk2004/firmware_lx2160ardb_rev2_uboot_xspiboot.img

 

From this, I get from booting my board this output (have a look about version)

U-Boot 2021.04-ge2eba0cd58 (Aug 27 2021 - 22:24:12 +0800)

...

load Standard DTB, VxWorks, apply DPL : all is OK

and I could not launch my VxWorks ! 

 

What's going on ?

 

WindRiver has same board as mine, all is same, vxworks is well launched

the only difference is about Uboot version : 

U-Boot 2020.04-00006-g0f2cfcb048 (Apr 19 2021 - 22:20:08 +0530)

 

My question is How can I get the binary relevant to "U-Boot 2020.04-00006-g0f2cfcb048"  ?

 

Thanks for any help on this

Best regard

Thierry LOUSSOT

 

 

 

 

 

 

0 Kudos
Reply
3 Replies

2,001 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please ask WindRiver for their u-boot to boot VxWorks.

The u-boot provided in NXP released SDK only can be used to boot Linux Kernel.

0 Kudos
Reply

1,989 Views
Thierry_LOUSSOT
Contributor II

Hi yipingwang

thanks for your answer

see with WindRiver, when booting, they get on output:

"U-Boot 2020.04-00006-g0f2cfcb048 (Apr 19 2021 - 22:20:08 +0530)"

where can I find this expected Uboot version ?

From many PDF versions (LSDKUG_RevYY.MM.pdf), I get differents links but not any idea about the Uboot version : 

https://www.nxp.com/lgfiles/sdk/lsdk2012/firmware_lx2160ardb_rev2_uboot_xspiboot.img

https://www.nxp.com/lgfiles/sdk/lsdk2108/firmware_lx2160ardb_rev2_xspiboot.img

Thanks for your answer

Best regards

Thierry LOUSSOT

0 Kudos
Reply

1,949 Views
yipingwang
NXP TechSupport
NXP TechSupport

U-Boot 2020.04 is released in LSDK 20.12 release, so please download pre-built image from 

https://www.nxp.com/lgfiles/sdk/lsdk2012/firmware_lx2160ardb_rev2_uboot_xspiboot.img

0 Kudos
Reply