frdm-ls1012a reset LED not off

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

frdm-ls1012a reset LED not off

1,945件の閲覧回数
bastian_schick
Contributor IV

Hi, on my Rev. B1 board the reset LED (D3) is never completely off.

The system is booting but I cannot connect to the board using Lauterbach and I wonder

a) is this normal that the LED is never completely off?

b) is someone able to debug the LS1012A through JTAG?

Cheers,

42Bastian

ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,761件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please download and install CodeWarrior for ARMv8 from CodeWarrior ARMv8 64 bit|NXP , and try whether you could connect to the target board through cmsis-dap, if you don't have a CodeWarrior TAP.

Thanks,

Yiping

0 件の賞賛
返信

1,761件の閲覧回数
sinanakman
Senior Contributor III

Hi Bastian

Regarding your question : "b) is someone able to debug the LS1012A through JTAG?"

I just wanted to let you know that I was able to debug LS1012A using BDI3000 JTAG debugger 

sometimes ago.

Hope this helps

Regards

Sinan Akman

1,761件の閲覧回数
addiyi
NXP Employee
NXP Employee

D3 should be off when RCW is loaded be the SoC. Are you saying D3 is on but uboot is booting?

LS1012AFRDM board can be debugger via cmsis-dap port as well via jtag port. I never tried with Lauterbach, but the support is added in CodeWarrior for ARMv8.

Adrian

0 件の賞賛
返信