Management Signals for SERDES in LS1021A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Management Signals for SERDES in LS1021A

1,857 Views
deepaknaiknavar
Contributor II

Hello,

Is it required to provide Management signals (MDC/MDIO) to the external PHY device for the SGMII interface in LS1021A? I mean does the Serdes interface itself can be used for the configuration PHY chip instead of the MDC/MDIO signals?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,727 Views
bpe
NXP Employee
NXP Employee

SGMII specification provides only for transferring  link status updates
over the SGMII link. Refer to SGMII Spesc, Section "Control Information
Exchanged Between Links". There are no provisions for setting or reading
any PHY register over SGMII. Thus, if you wish to have full control
over your PHY, yes,  you need to connect it to an out-of-band management
interface.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,727 Views
erdani80
Contributor III

Probably you could have a look at theTBI registers inside the eTSEC controller.

If you are planning to use a SFP you could also use fixed phy controllers in linux to get a connection.

0 Kudos
Reply