Hi,
I have and older v1.0 ls1021a-iot from technexion. I also have a v2.0 which is working great with the latest u-boot (2017.01) and linux kernel (4.9). If i use the latest u-boot on the v1.0 board, I do not see any u-boot output.
Can anybody PLEASE help me to get u-boot working on it?
Thanks
LJ
Hi Leon
Mainline u-boot support for this board was added only recently. Would you be able to send
an e-mail to u-boot mailing list and report the problem with v1.0 board ? Please make sure
York Sun (york.sun at nxp.com) is also cc'ed.
Thanks and best regards
Sinan Akman
SDK 1.7 and SDK 1.8 support the LS1021a rev 1.
Usually the LS1021a-IOT board contains the LS1021A-IOT-Rev-B-SDK-0.4. This SDK supports the LS1021a rev 1.
Have a great day,
Pavel Chubakov
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------