flash_Algorithm_template for Ls1043a custom board with Flash MT28FW02GBBA1H

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

flash_Algorithm_template for Ls1043a custom board with Flash MT28FW02GBBA1H

4,096件の閲覧回数
perumandlasairam1064
Contributor I

Hi all

we are working with LS1043A processor in our custom board. In LS1043ARDB the flash used is MT28EW01GABA1H  and we are using the flash in custom board is MT28FW02GBBA1HPC.

My question is "Is the flash(MT28EW01GABA1H ) Algorithm of  LS1043ARDB can use for flash(MT28FW02GBBA1HPC) of custom board"? 

I added the new .xml in devices, algorithms and params for  MT28FW02GBBA1HPC but when I am trying to program flash the error "id verify fail" is comming.

Now I need to create a flash Algorithm for flash, for that I installed flash tool kit , but I need a example flash template for Algorithm_template to make our own flash algorithm for custom board.

I am attaching screen shots, what I did up to.

Thank you.

0 件の賞賛
返信
0 返答(返信)