LS1012A LSDK 21.08 insmod fail!!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS1012A LSDK 21.08 insmod fail!!

1,246件の閲覧回数
Gyosun
Contributor III

Hello,

I have successfully ported LSDK 21.08 to my custom board, LS1012AFRWY. When I tried to compile and insmod the module driver that was used with the previous LSDK 18.12, it appears that the kernel version is not compatible.

I have written the Makefile as follows, and it compiled successfully, resulting in the generation of the .ko file.

DEVNAME := dev_pci_xdma_ls1012a

obj-m += $(DEVNAME).o

$(DEVNAME)-objs := main.o

PWD := $(shell pwd)
KDIR := /home/yhoh/wk-cleverlogic-LayerscapeSDK/flexbuild/build/linux/linux/arm64/LS/output/LSDK-21.08

all:
make -C $(KDIR) M=$(PWD) clean
make CROSS_COMPILE=aarch64-linux-gnu- ARCH=arm64 -C $(KDIR) M=$(PWD) modules


clean:
make -C $(KDIR) M=$(PWD) clean

 

After copying the file to the board and issuing the insmod command, it doesn't seem to be functioning correctly.

[root@LSDK ~]# insmod dev_pci_xdma_ls1012a.ko
[ 1838.387700] dev_pci_xdma_ls1012a: loading out-of-tree module taints kernel.
[ 1838.399196] kboject example_init() done. ret=0
[root@LSDK ~]# uname -a
Linux LSDK 5.10.35-dirty #1 SMP PREEMPT Wed Oct 4 18:44:39 KST 2023 aarch64 GNU/Linux

 

Please provide instructions on how to compile and run a module separately, without integrating it into the kernel.

Thank you.
Best Regards,
Gyosun.

0 件の賞賛
返信
1 返信

1,219件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Sorry, the kernel is not compatible with your module, you have to build the whole module with the kernel version that you are using otherwise it simple won't work.

regards

0 件の賞賛
返信