flash_Algorithm_template for Ls1043a custom board with Flash MT28FW02GBBA1H

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flash_Algorithm_template for Ls1043a custom board with Flash MT28FW02GBBA1H

4,042 Views
perumandlasairam1064
Contributor I

Hi all

we are working with LS1043A processor in our custom board. In LS1043ARDB the flash used is MT28EW01GABA1H  and we are using the flash in custom board is MT28FW02GBBA1HPC.

My question is "Is the flash(MT28EW01GABA1H ) Algorithm of  LS1043ARDB can use for flash(MT28FW02GBBA1HPC) of custom board"? 

I added the new .xml in devices, algorithms and params for  MT28FW02GBBA1HPC but when I am trying to program flash the error "id verify fail" is comming.

Now I need to create a flash Algorithm for flash, for that I installed flash tool kit , but I need a example flash template for Algorithm_template to make our own flash algorithm for custom board.

I am attaching screen shots, what I did up to.

Thank you.

0 Kudos
Reply
0 Replies