error in creating bitbake image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error in creating bitbake image

1,418 Views
venkataramana1
Contributor I

Hii,

I am using UBUNTU_20.04_FLEXBUILD_YOCTO_TINY

initially i have created a hello.c file and using cross compiled  it generates the object file.  later i copied this object file into  the path: home/icomm/distro/build-ls1043ardb/sources/meta-freescale/recipes-extended/merge-files/merge-files/merge. 

Changed  the  fsl-image-mfgtool.bb   to  include  the  merge-files

LICENSE = "MIT"

IMAGE_INSTALL:append = " \

    packagegroup-core-ssh-dropbear \

    packagegroup-fsl-mfgtools \

    udev-extraconf \

    file \

    parted \

    lmsensors-sensors \

    restool \

    fmc \

    sudo \

    curl \

    merge-files \

"

IMAGE_INSTALL:remove:ls1021atwr = "restool"

 

PACKAGE_EXCLUDE = "kernel-image-*"

 

export IMAGE_BASENAME = "fsl-image-mfgtool"

 

IMAGE_ROOTFS_EXTRA_SPACE = "262144"

 

In the bb file following script is present

DESCRIPTION = "Merge prebuilt/extra files into rootfs"

LICENSE = "MIT"

LIC_FILES_CHKSUM = "file://${COREBASE}/meta/COPYING.MIT;md5=3da9cfbcb788c80a0384361b4de20420"

 

inherit allarch

 

SRC_URI = "file://merge"

S = "${WORKDIR}"

 

MERGED_DST ?= "${ROOT_HOME}"

do_install () {

    install -d ${D}/${MERGED_DST}

    find ${WORKDIR}/merge/ -maxdepth 1 -mindepth 1 -not -name README \

    -exec cp -fr '{}' ${D}/${MERGED_DST}/ \;

    find ${WORKDIR}/merge/ -maxdepth 1 -mindepth 1 -exec rm -fr '{}' \;

}

do_configure[noexec] = "1"

do_compile[noexec] = "1"

 

FILES:${PN} = "/*"

ALLOW_EMPTY:${PN} = "1"

INSANE_SKIP:${PN} = "debug-files dev-so"

 

 later i have run the command : bitbake fsl-image-mfgtool

i am getting following error:

Loaded 4803 entries from dependency cache.

ERROR: ParseError at /home/icomm/distro/sources/meta-freescale/recipes-extended/merge-files/merge-files_1.0.bb:5: Could not inherit file classes/arch64.bbclass

ERROR: Parsing halted due to errors, see error messages above

 

Summary: There were 2 ERROR messages, returning a non-zero exit code.

please any one help me to resolve this issue

0 Kudos
Reply
1 Reply

1,373 Views
yipingwang
NXP TechSupport
NXP TechSupport

Would you please provide detailed information?

Which "layerscape Linux distribution" are you using? Is it released by NXP? Where did you download it?
I want to do verification on my build machine.

In addition, it is weird that why source recipe folder was deployed in build project folder build-ls1043ardb in your build environment.

0 Kudos
Reply