core voltage not adjusted

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

core voltage not adjusted

跳至解决方案
1,537 次查看
muaxi8
Contributor V

LX2080a custom board.

The Uboot print has one line output:  core voltage not adjusted。

Is this a voltage adjustment for the CPU core ?

Is there any problem with this adjustment failure? My board is now unable to Bringing up secondary CPUs. Is it related to this ?

muaxi8_0-1628589415690.png

 

标记 (1)
0 项奖励
回复
1 解答
1,531 次查看
ufedor
NXP Employee
NXP Employee

You wrote:

> Is this a voltage adjustment for the CPU core ?

Yes.

During the system initialization VID is read from the processor to adjust VDD accordingly.

> Is there any problem with this adjustment failure?

When VDD is not adjusted then power consumption could be non-optimal (higher), but there could not be functional issues.

> My board is now unable to Bringing up secondary CPUs. Is it related to this ?

Not related.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,532 次查看
ufedor
NXP Employee
NXP Employee

You wrote:

> Is this a voltage adjustment for the CPU core ?

Yes.

During the system initialization VID is read from the processor to adjust VDD accordingly.

> Is there any problem with this adjustment failure?

When VDD is not adjusted then power consumption could be non-optimal (higher), but there could not be functional issues.

> My board is now unable to Bringing up secondary CPUs. Is it related to this ?

Not related.

0 项奖励
回复