core voltage not adjusted

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

core voltage not adjusted

Jump to solution
1,539 Views
muaxi8
Contributor V

LX2080a custom board.

The Uboot print has one line output:  core voltage not adjusted。

Is this a voltage adjustment for the CPU core ?

Is there any problem with this adjustment failure? My board is now unable to Bringing up secondary CPUs. Is it related to this ?

muaxi8_0-1628589415690.png

 

0 Kudos
Reply
1 Solution
1,533 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> Is this a voltage adjustment for the CPU core ?

Yes.

During the system initialization VID is read from the processor to adjust VDD accordingly.

> Is there any problem with this adjustment failure?

When VDD is not adjusted then power consumption could be non-optimal (higher), but there could not be functional issues.

> My board is now unable to Bringing up secondary CPUs. Is it related to this ?

Not related.

View solution in original post

0 Kudos
Reply
1 Reply
1,534 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> Is this a voltage adjustment for the CPU core ?

Yes.

During the system initialization VID is read from the processor to adjust VDD accordingly.

> Is there any problem with this adjustment failure?

When VDD is not adjusted then power consumption could be non-optimal (higher), but there could not be functional issues.

> My board is now unable to Bringing up secondary CPUs. Is it related to this ?

Not related.

0 Kudos
Reply