code warrior tap error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

code warrior tap error

11,502件の閲覧回数
rashmikj
Contributor III

Hi,

When i try to connect code warrior tap to LS1046ardb , I am getting the following error.

Kindly help

タグ(1)
0 件の賞賛
返信
6 返答(返信)

11,492件の閲覧回数
ufedor
NXP Employee
NXP Employee

Which Target Configuration is selected?

Run Diagnose Connection:

Diagnose.jpg

 

0 件の賞賛
返信

11,482件の閲覧回数
rashmikj
Contributor III

Please find attached error also when i scan for probe its unable to scan the codewarrior tap usb connected.

0 件の賞賛
返信

11,478件の閲覧回数
ufedor
NXP Employee
NXP Employee

Press "Connection Diagnostics" button and provide the Connection Diagnostics tab screenshot.

0 件の賞賛
返信

11,470件の閲覧回数
rashmikj
Contributor III

Please find attached screenshot.

0 件の賞賛
返信

11,464件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please try the following steps:

1) completely uninstall CodeWarrior IDE

2) disable anti-virus application(s)

3) install latest Java

4) install CodeWarrior IDE

5) enable anti-virus application(s)

 

In case of further questions capture complete Help message as text.

0 件の賞賛
返信

11,455件の閲覧回数
rashmikj
Contributor III

After disabling the anti virus and reinstalling the code warrior , it is working fine.

Thank you.

タグ(1)
0 件の賞賛
返信