code warrior tap error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

code warrior tap error

11,255 Views
rashmikj
Contributor III

Hi,

When i try to connect code warrior tap to LS1046ardb , I am getting the following error.

Kindly help

Tags (1)
0 Kudos
Reply
6 Replies

11,245 Views
ufedor
NXP Employee
NXP Employee

Which Target Configuration is selected?

Run Diagnose Connection:

Diagnose.jpgDiagnose.jpg

0 Kudos
Reply

11,235 Views
rashmikj
Contributor III

Please find attached error also when i scan for probe its unable to scan the codewarrior tap usb connected.

0 Kudos
Reply

11,231 Views
ufedor
NXP Employee
NXP Employee

Press "Connection Diagnostics" button and provide the Connection Diagnostics tab screenshot.

0 Kudos
Reply

11,223 Views
rashmikj
Contributor III

Please find attached screenshot.

0 Kudos
Reply

11,217 Views
ufedor
NXP Employee
NXP Employee

Please try the following steps:

1) completely uninstall CodeWarrior IDE

2) disable anti-virus application(s)

3) install latest Java

4) install CodeWarrior IDE

5) enable anti-virus application(s)

 

In case of further questions capture complete Help message as text.

0 Kudos
Reply

11,208 Views
rashmikj
Contributor III

After disabling the anti virus and reinstalling the code warrior , it is working fine.

Thank you.

Tags (1)
0 Kudos
Reply