Yocto build vpp

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Yocto build vpp

911 次查看
Blue_Sky1
Contributor II

Hi,

I refer to section 8.3.4.2 of the LLDP_6.1.55_2.2.0 documentation for the build vpp,used command:bitbake vpp,a very large number of rpm packages related to vpp have been generated in the following folder。

1、is this normal?Because in lsdk21.08, vpp will only generate 9 relevant deb package files.

2、How do I install vpp?

/root/yocto/build_lx2160ardb-rev2/tmp/work/aarch64-fsl-linux/vpp/2302-r0/deploy-rpms/aarch64

stupid_0-1722246315024.png

 

0 项奖励
回复
2 回复数

888 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Yes  it is normal because is the dependencies of yocto and your apps. if you are in yocto, you have to build the whole package once it added to it.

regards

0 项奖励
回复

869 次查看
Blue_Sky1
Contributor II
Hi,Bio_TICFSL

Yes,i build vpp in yocto system,and i just run this command:bitbake vpp.

How do I take the compiled vpp and install it on the lx2160?

Thanks
0 项奖励
回复