Using our board with LS1043 processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using our board with LS1043 processor

1,138 Views
carlos-m-ribeiro
Contributor I

Good morning,

If possible we would like to clarify a matter with NXP and we need your help.

In our company, we will have an real scenario that uses ls1043 processor in our boards. If we need only to use the U-BOOT for QSPI, the Frame Manager's (FMan), the Period and Pulse Accumulator (PPA) and the Reset Configuration Word (RCW), which should be the most recommended command ls1043aqds of flex-builder and which binaries should be flash into our board. Another important thing is to know which files are dedicated to our board.

 

Best regards

 

 

0 Kudos
Reply
3 Replies

1,116 Views
ufedor
NXP Employee
NXP Employee

> Period and Pulse Accumulator (PPA)

PPA means Primary Protected Application. It is not supported for the LS1043A in the latest LSDK.

Considering requested functionality it will be supported by the composite firmware image generated by flexbuilder - please read the Layerscape Linux SDK Documentation:

https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/layerscap...

 

0 Kudos
Reply

1,113 Views
carlos-m-ribeiro
Contributor I

Thank you for your response but there was a mistake. All we need for our board is the frame manager, U-BOOT and RCW+PBI=PBL.

Best regards

0 Kudos
Reply

1,130 Views
carlos-m-ribeiro
Contributor I

NOTE: our board also need PBI-PBL.

0 Kudos
Reply