Unable to enable Interactive DDR debugging with LS1043A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Unable to enable Interactive DDR debugging with LS1043A

5,403件の閲覧回数
jerrymorrow
Contributor III

Hello,

I'm trying to get the 'Interactive DDR debugging' (FSL DDR> prompt) working with our LS1043ARDB development board.  I have more than a month of experience working with the SDK 2.0 (plus patch) with this development board.

Some slides from our NXP training state the CONFIG_FSL_DDR_INTERACTIVE conditional compile flag must be set, and rebuild u-boot.  Is this necessarily for the default build? 

I found a README.fsl-ddr file in this directory:

./build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/u-boot-qoriq/2016.01+fslgit-r0/git/doc

It states two different ways to enable the FSL DDR debug prompt (set environment variable, and/or press 'd' on reset), and neither of them work.

Jerry

ラベル(1)
3 返答(返信)

5,037件の閲覧回数
hawkin
Contributor II

@Jerry Morrow  I define  environment variable <ddr_interactive> as fellow:

setenv ddr_interactive 1

saveenv

reset

then can entry DDR debug mode automatic.

i can't entry DDR debug mode by entry "d"

see reference doc: README.fsl-ddr

0 件の賞賛
返信

5,033件の閲覧回数
allen_j_andreu
Contributor I

hawkin wrote:

@Jerry Morrow  I define  environment variable <ddr_interactive> as fellow:

setenv ddr_interactive 1

saveenv

reset

then can entry DDR debug mode automatic.

 

i can't entry DDR debug mode by entry "d"

see reference doc: README.fsl-ddr

I set ddr_interactive = 1 and enabled the common debug option for uboot and still do not get to the ddr debugger prompt.

0 件の賞賛
返信

5,031件の閲覧回数
Pavel
NXP Employee
NXP Employee

This option is enabled in default configuration of the LS1043ARDB u-boot.

Attached file contains the LS1043ADRB u-boot configuration file and screenshot if 'd' is pressed during u-boot starting.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------