TWR-LS1021A USB STANDALONE MODE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-LS1021A USB STANDALONE MODE

ソリューションへジャンプ
3,798件の閲覧回数
JHY
Contributor IV

I heard that LS1021A has usb controller can be configured as host or device.

But default setting of TWR-1021A is not device mode, I think.

How can I operate it as a stand-alone USB device?

Best regards.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,555件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

USB 3.0 controller is connected to USB 3.0 hub on the TWR board, because of this reason the only host mode is available on this board.

USB 2.0 controller is available via elevator board and can be used in both modes.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,556件の閲覧回数
alexander_yakov
NXP Employee
NXP Employee

USB 3.0 controller is connected to USB 3.0 hub on the TWR board, because of this reason the only host mode is available on this board.

USB 2.0 controller is available via elevator board and can be used in both modes.

0 件の賞賛
返信