TWR-LS1021A USB STANDALONE MODE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-LS1021A USB STANDALONE MODE

Jump to solution
3,820 Views
JHY
Contributor IV

I heard that LS1021A has usb controller can be configured as host or device.

But default setting of TWR-1021A is not device mode, I think.

How can I operate it as a stand-alone USB device?

Best regards.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
3,577 Views
alexander_yakov
NXP Employee
NXP Employee

USB 3.0 controller is connected to USB 3.0 hub on the TWR board, because of this reason the only host mode is available on this board.

USB 2.0 controller is available via elevator board and can be used in both modes.

View solution in original post

0 Kudos
Reply
1 Reply
3,578 Views
alexander_yakov
NXP Employee
NXP Employee

USB 3.0 controller is connected to USB 3.0 hub on the TWR board, because of this reason the only host mode is available on this board.

USB 2.0 controller is available via elevator board and can be used in both modes.

0 Kudos
Reply