TSN Switch problem with OpenIL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TSN Switch problem with OpenIL

2,035 Views
ainolike
Contributor III

Hi,

I have some problem when using LS1028A TSN switch. The TSN Switch configuration as follows in Linux.

ip link set eno2 up

ip link add name switch type bridge

ip link set dev swp0 master switch && ip link set swp0 up

ip link set dev swp1 master switch && ip link set swp1 up

ip link set dev swp2 master switch && ip link set swp2 up

ip link set dev swp3 master switch && ip link set swp3 up

ifconfig switch 192.168.1.100

When using openil-v1.10, if I plug in the network cable first and then configure the command, I can ping the host at the other end of the network. If I configure the command first and then plug in the network cable, I cannot ping the host at the other end of the network, but after I plug in the network cable again, I can ping the host at the other end of the network.

When using LSDK2004, no matter I configure the command first or plug in the network cable, it can ping normally.

0 Kudos
Reply
2 Replies

1,993 Views
ainolike
Contributor III

The PHY chip has been linked up, but the LINK_STAT bit of QSGMII Status Register is still 0. Why does this bit not change?In what circumstances will it change?

0 Kudos
Reply

2,007 Views
ainolike
Contributor III

Hi,

I found it is because the value of MDIO_QSGMII  status register still 0x9. Why does this register take effect on linking up. My PHY connects to EMDIO.

0 Kudos
Reply