TFTP in binary mode? ls1021a-twr

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TFTP in binary mode? ls1021a-twr

ソリューションへジャンプ
3,496件の閲覧回数
datho
Contributor III


I'm currently using a ls1021a-twr rev 2 board, that has a tftp command (GNU inetutils 1.9.2). This tftp command doesn't have a way to specify a binary mode. When I tftp files from Linux it works just fine but I also want to tftp files from a Windows server. Without the binary mode for the tftp, a lot of the files I get from Windows become unusable.

Is there a way to update the tftp command to allow for binary mode? or is there another way to get files from a windows machine without corrupting them?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,075件の閲覧回数
ufedor
NXP Employee
NXP Employee

Use "binary" command for the binary transfer mode:

GNU Inetutils: tftp invocation

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,076件の閲覧回数
ufedor
NXP Employee
NXP Employee

Use "binary" command for the binary transfer mode:

GNU Inetutils: tftp invocation

0 件の賞賛
返信