TFTP in binary mode? ls1021a-twr

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TFTP in binary mode? ls1021a-twr

Jump to solution
4,534 Views
datho
Contributor III


I'm currently using a ls1021a-twr rev 2 board, that has a tftp command (GNU inetutils 1.9.2). This tftp command doesn't have a way to specify a binary mode. When I tftp files from Linux it works just fine but I also want to tftp files from a Windows server. Without the binary mode for the tftp, a lot of the files I get from Windows become unusable.

Is there a way to update the tftp command to allow for binary mode? or is there another way to get files from a windows machine without corrupting them?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
4,113 Views
ufedor
NXP Employee
NXP Employee

Use "binary" command for the binary transfer mode:

GNU Inetutils: tftp invocation

View solution in original post

0 Kudos
Reply
1 Reply
4,114 Views
ufedor
NXP Employee
NXP Employee

Use "binary" command for the binary transfer mode:

GNU Inetutils: tftp invocation

0 Kudos
Reply