Setting up multiple VLANs on a LX2160

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting up multiple VLANs on a LX2160

1,236 次查看
Ncaseau
Contributor I

Hi !

Is it possible to configure multiple VLANs on a ethernet port of the LX2160 board ? I would like to be able to setup a switch that receives packets on a port and forwards them to two other ports based on the VLAN ID inside the packet.

I it is possible, could you explain to me how to set it up ?

Thank you.

Have a good day,

Nicolas

 

0 项奖励
回复
1 回复

1,195 次查看
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Yes it is possible, the DPSW component provides VLAN filtering.

take a look in the DPAA2 user manual, DPSW_CREATE command takes a 16bit MAX_VLANS.

You can also find examples of Setting up Ethernet Switch Capability in the LSDK 21.08 USER GUIDE

0 项奖励
回复