Setting up multiple VLANs on a LX2160

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting up multiple VLANs on a LX2160

1,234 Views
Ncaseau
Contributor I

Hi !

Is it possible to configure multiple VLANs on a ethernet port of the LX2160 board ? I would like to be able to setup a switch that receives packets on a port and forwards them to two other ports based on the VLAN ID inside the packet.

I it is possible, could you explain to me how to set it up ?

Thank you.

Have a good day,

Nicolas

 

0 Kudos
Reply
1 Reply

1,193 Views
Oswalag
NXP TechSupport
NXP TechSupport

Hello,

Yes it is possible, the DPSW component provides VLAN filtering.

take a look in the DPAA2 user manual, DPSW_CREATE command takes a 16bit MAX_VLANS.

You can also find examples of Setting up Ethernet Switch Capability in the LSDK 21.08 USER GUIDE

0 Kudos
Reply