Setting the basetime failed on the ls1028 platform

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Setting the basetime failed on the ls1028 platform

515 次查看
Eddy1
Contributor V

Hi:

Recently, while testing basetime with the qbv tool on the ls1028 platform, unfortunately, the ports from the vsc8514 switch cannot set the basetime. For example, when setting the current time to 99ms, the actual time decreases sequentially from 99 to 0, cyclically repeating. Below are the steps of my test:

1)qbv config

root@localhost:~# cat > qbv1.txt << EOF

> t0 11111111b 10000

> t1 00000000b 99990000

> EOF

2)Get ptp time

tsntool> ptptool -g

ptp time: 26122.620341052

3)set basetime

tsntool> qbvset --device swp1 --entryfile qbv1.txt --basetime 26123.666

tsntool> quit

 ping 192.168.2.101 -s 1000 

PING 192.168.2.3 (192.168.2.3): 1000 data bytes

Eddy1_0-1711366632256.png

Please provide the corresponding suggestions.

0 项奖励
回复
0 回复数