Set CPU frequency not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set CPU frequency not working

Jump to solution
161 Views
noahw
Contributor III

I am following directions on this page (https://docs.nxp.com/bundle/GUID-39A0A446-70E5-4ED7-A580-E7508B61A5F1/page/GUID-40BE9AD5-DF6B-4D99-A...) about switching CPU frequency by writing to a file in /sys.

When I try to run the command

echo 799999 > /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed

I see the following error:

-bash: echo: write error: Invalid argument

 

What am I doing wrong? I tried other values like 300000, and I also tried putting the value in quotes, using the -n flag for echo, etc. I used chmod to add write permission to scaling_setspeed. Is there something else I need to do?

0 Kudos
Reply
1 Solution
115 Views
June_Lu
NXP TechSupport
NXP TechSupport

In the default LSDK2108.

root@localhost:~# cd /sys/devices/system/cpu/cpu0/cpufreq

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# ls

affected_cpus     cpuinfo_max_freq  cpuinfo_transition_latency  scaling_available_frequencies  scaling_cur_freq  scaling_governor  scaling_min_freq  stats

cpuinfo_cur_freq  cpuinfo_min_freq  related_cpus                scaling_available_governors    scaling_driver    scaling_max_freq  scaling_setspeed

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_available_governors

ondemand userspace performance

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# echo userspace > scaling_governor

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_cur_freq

600000

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_available_frequencies

1500000 1200000 750000 600000 375000 300000

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# echo 750000 > scaling_setspeed

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_cur_freq

750000

View solution in original post

0 Kudos
Reply
3 Replies
116 Views
June_Lu
NXP TechSupport
NXP TechSupport

In the default LSDK2108.

root@localhost:~# cd /sys/devices/system/cpu/cpu0/cpufreq

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# ls

affected_cpus     cpuinfo_max_freq  cpuinfo_transition_latency  scaling_available_frequencies  scaling_cur_freq  scaling_governor  scaling_min_freq  stats

cpuinfo_cur_freq  cpuinfo_min_freq  related_cpus                scaling_available_governors    scaling_driver    scaling_max_freq  scaling_setspeed

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_available_governors

ondemand userspace performance

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# echo userspace > scaling_governor

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_cur_freq

600000

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_available_frequencies

1500000 1200000 750000 600000 375000 300000

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# echo 750000 > scaling_setspeed

root@localhost:/sys/devices/system/cpu/cpu0/cpufreq# cat scaling_cur_freq

750000

0 Kudos
Reply
145 Views
June_Lu
NXP TechSupport
NXP TechSupport

Please kindly share the MPU part number and SW version, thanks

0 Kudos
Reply
131 Views
noahw
Contributor III

@June_Lu This is the LS1028ARDB running LSDK 21.08, kernel 5.10.35.

0 Kudos
Reply