Schematic & Reference manual mismatch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Schematic & Reference manual mismatch

ソリューションへジャンプ
3,249件の閲覧回数
TrinathK
Contributor III

Hi all,

In LS1046A reference manual, it is mentioned that, QSPI_A_DATA[3] pin should be pulled low when IFC_GRP_A_EXT is selected as 001 (i.e., when pin is used as QSPI_A_DATA[3]). But in the schematics provided, it is not pulled low.  Please check and confirm if pull down is required or not.

Attached images (text is highlighted) for your reference.

Thanks in advance.

0 件の賞賛
返信
1 解決策
3,220件の閲覧回数
r8070z
NXP Employee
NXP Employee

Please see also Table 25. QSPI pin termination checklist in the QorIQ LS1046A Design Checklist , Rev. 2, 06/2020. Pull down for QSPI_A_DATA[3] is not required.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,236件の閲覧回数
TrinathK
Contributor III

Hi Serguei,

Thanks for the reply.

So you are saying, pull down is applicable only for reserved pins and not for QSPI_A_DATA[3]. But the NOTE mentioned in the reference manual, looks like it is applicable for all the pins mentioned (i.e., QSPI_A_DATA[3], Reserved, Reserved). Please confirm if pull down is required for QSPI_A_DATA[3] or not.

Thanks in advance.

0 件の賞賛
返信
3,221件の閲覧回数
r8070z
NXP Employee
NXP Employee

Please see also Table 25. QSPI pin termination checklist in the QorIQ LS1046A Design Checklist , Rev. 2, 06/2020. Pull down for QSPI_A_DATA[3] is not required.

0 件の賞賛
返信
3,239件の閲覧回数
r8070z
NXP Employee
NXP Employee

“001 {QSPI_A_DATA[3], Reserved, Reserved} NOTE: Must be pulled low when IFC_GRP_A_EXT is selected as 001“ means that when IFC_GRP_A_EXT is selected as 001 there are 2 reserved pins which must be pulled low.

Attached schematics looks like LS1046ARDB which was designed using preliminary documentation Due to that it shows these 2 pins as QSPI_A_DQS and QSPI_B_DQS. We should follow to the manual recommendation.

0 件の賞賛
返信