[LS1046 / Customer Sanmina] OS boot failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

[LS1046 / Customer Sanmina] OS boot failure

2,514 次查看
srinivas_chilaka
NXP Employee
NXP Employee

Hi,

 

Customer has reported that they have 1 unit of LFHP1824-1290 failed at FCT station. We need your help for this analysis. Appreciate your support in this request.  

 

Below are the details of the affected unit:

 

Part Number : LFHP1824-1290

MPN : LS1046ASE8T1A

Description : IC QORIQ PROCESSOR 4 CORES 780-FCPBGA

Supplier : NXP Semiconductors

Date Code : 2114

Location on Board : U83

Board S/N : SG17KPK013

Fail Station : FCT

Failure Description : Able to load RCW and Uboot, but unable to load OS and boot further.

 

 RCW – Reset configuration word.

Reset Configuration Word (RCW):

       00000000: 0e150012 0d000000 00000000 00000000

       00000010: 33335577 0000401e 40000000 c1000000

       00000020: 00000000 05000100 00000000 00428ffd

       00000030: 00004104 24101200 00000096 00000001

 

 Read existing content (codes) – store for future reference:

No issue with the code/flash, as the board able to pass all flash partition and functionalities check with new processor.

 

 Reflash and reverify the content (code): 

Same code/flash works on a new processor, which means no issue with the code or flash.

 

Reverify board functionality:

Board functionality good with new processor

 

   Like at what voltage, what temperature, how to translate that the RCW message into failure description.

=> voltage - 3.3V, 1.8V,1.2V

=> room temp 

=>  Customer: I mentioned RCW just to say that Processor has crossed the initial milestone of booting up using the Uboot from the SPI flash. it got hanged while booting up to the OS from the emmc interface. RCW itself don’t have an error code within it. Need to get NXP to perform their full chip level test and confirm no issues on their side.

0 项奖励
回复
3 回复数

2,500 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Would you please provide the customer's console log to boot OS?

Has the customer used QCVS DDRv tool to connect to the custom board to do optimization and validation?

0 项奖励
回复

2,490 次查看
srinivas_chilaka
NXP Employee
NXP Employee

@yipingwang Thanks for the reply. I'm checking with the customer.

Do you find any error in the RCW provided by the customer?

 

RCW – Reset configuration word.

Reset Configuration Word (RCW):

00000000: 0e150012 0d000000 00000000 00000000

00000010: 33335577 0000401e 40000000 c1000000

00000020: 00000000 05000100 00000000 00428ffd

00000030: 00004104 24101200 00000096 00000001

0 项奖励
回复

2,485 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Please suggest customer customize RCW with LSDK.

Please download the latest LSDK 2108.

$ source setup.env

$ flex-builder -c rcw -m ls1046ardb

Then modify *.rcw in components/firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/.

Rebuild RCW with the following command and get rcw*.bin in components/firmware/rcw/ls1046ardb/RR_FFSSPPPH_1133_5559/.

$ flex-builder -c rcw -m ls1046ardb

0 项奖励
回复