SGMII reference clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SGMII reference clock

4,251 次查看
thomas_delgrand
Contributor I

Which is the frequency for the SerDes reference clock when using SGMII in the LS1012A?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

3,844 次查看
r8070z
NXP Employee
NXP Employee

Have a great day,

For SGMII (1.25 GBaud) the SerDes reference clock frequency is 100MHz or 125MHz. For SGMII (3.125 GBaud) the SerDes reference clock frequency is 125MHz. See Table 27-3 in the LS1012A reference manual rev.0.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复