SGMII reference clock

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SGMII reference clock

4,233件の閲覧回数
thomas_delgrand
Contributor I

Which is the frequency for the SerDes reference clock when using SGMII in the LS1012A?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

3,826件の閲覧回数
r8070z
NXP Employee
NXP Employee

Have a great day,

For SGMII (1.25 GBaud) the SerDes reference clock frequency is 100MHz or 125MHz. For SGMII (3.125 GBaud) the SerDes reference clock frequency is 125MHz. See Table 27-3 in the LS1012A reference manual rev.0.

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信