SD card device setting in LS1021a

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SD card device setting in LS1021a

1,127 次查看
szlin
Contributor I

TWR-LS1021A equips SD card; however, the esdhc function is disabled in 1021a.dtsi and there is no overwrite setting in ls1021a-twr.dts.

But the SD function works well in TWR board, could you clarify this point?

标签 (1)
0 项奖励
回复
1 回复

967 次查看
Pavel
NXP Employee
NXP Employee

The LS1021a-twr.dts file contains the following:

                               esdhc@1560000 {

                                               compatible = "fsl,ls1021a-esdhc", "fsl,esdhc";

                                               reg = <0x0 0x1560000 0x0 0x10000>;

                                               interrupts = <0x0 0x5e 0x4>;

                                               clock-frequency = <0x0>;

                                               voltage-ranges = <0x708 0x708 0xce4 0xce4>;

                                               sdhci,auto-cmd12;

                                               big-endian;

                                               bus-width = <0x4>;

                                               rcpm-wakeup = <0x3 0x80 0x0>;

                                               status = "disabled";

                               };

 

“disabled” - Indicates that the device is not presently operational, but it might become operational in the future (for example, something is not plugged in, or switched off).

Refer to the device binding for details on what disabled means for a given device.

 

See the following document:

http://elinux.org/images/c/cf/Power_ePAPR_APPROVED_v1.1.pdf

 

It is correct status for SDHC since often SD card is not plugged in.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复