Running Packet Reflector AIOP App

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Running Packet Reflector AIOP App

3,639件の閲覧回数
janarbek_matai
Contributor III

HI All,

I am trying to run the packet reflector AIOP app on my LS1088ARDB board.

I did follow the instructions from LSDK Reference Manual Rev. 18.09 Section: Running the Reflector Application. Section nubmer:   8.3.7.1.2.2

Here are the steps presented in the manual:

./dynamic_aiop_only.sh
#aiop_tool load -g dprc.3 -f /usr/aiop/bin/aiop_reflector.elf &
#cat /dev/fsl_aiop_console | grep REFLECTOR
#busybox tail –f /dev/fsl_aiop_console   => This step does not show the results presented in the LSDK Refence manual. See the attached busybox.PNG.

I am not sure what I am doing wrong here. Please find the attached log of the commands aiop_reflector_log.txt

This is what I get:

root@ls1088ardb:~# busybox tail -f /dev/fsl_aiop_console
0x000001c0: 00000000 00000001 00000000 00000002
0x000001d0: 00000000 00000000 00000000 00000000
0x000001e0: 00000000 00000000 00000000 00000000
0x000001f0: 00000000 00000000 00000000 00000000
> TRACE [CPU 0, cmdif_srv.c:651 cmdif_srv_isr]: cmd_id = 0x1002
> TRACE [CPU 0, cmdif_srv.c:652 cmdif_srv_isr]: auth_id = 0x1
> TRACE [CPU 0, cmdif_srv.c:653 cmdif_srv_isr]: gpp_icid = 0x0
> TRACE [CPU 0, cmdif_srv.c:654 cmdif_srv_isr]: gpp_dma flags = 0xc000
REFLECTOR : NI 0 link is UP
> TRACE [CPU 0, cmdif_srv.c:775 cmdif_srv_isr]: PASSED No Response Command

This is what I expect:

RX on NI 0 | CORE:15
MAC_SA: 00-10-94-00-00-02 MAC_DA: 00-00-00-00-00-06
IP_SRC: 192.85.1.1 IP_DST: 192.0.0.1
RX on NI 0 | CORE:14
MAC_SA: 00-10-94-00-00-02 MAC_DA: 00-00-00-00-00-06
IP_SRC: 192.85.1.2 IP_DST: 192.0.0.1
. . .
RX on NI 0 | CORE:9
MAC_SA: 00-10-94-00-00-02 MAC_DA: 00-00-00-00-00-06
IP_SRC: 192.85.1.3 IP_DST: 192.0.0.1

ラベル(1)
0 件の賞賛
返信
1 返信

3,477件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Janarbek Matai,

It's seems that your test result is normal, please refer to the following log with LSDK 1812 images.

root@localhost:/mnt# ./dynamic_aiop_only.sh
restool LSDK-18.12
MC firmware version: 10.12.0
Disconnecting DPNIs to create AIOP connections
Creating AIOP Container
Assigned dpbp.0 to dprc.2
Assigned dpbp.2 to dprc.2
Assigned dpbp.3 to dprc.2
Assigned dpbp.4 to dprc.2
Assigned dpni.1 to dprc.2
Connecting dpni.1<------->dpmac.1
Assigned dpni.2 to dprc.2
Connecting dpni.2<------->dpmac.2
AIOP Container dprc.2 created
----- Contents of AIOP Container: dprc.2 -----
dprc.2 contains 7 objects:
object          label           plugged-state
dpni.2                          plugged
dpni.1                          plugged
dpbp.4                          plugged
dpbp.3                          plugged
dpbp.2                          plugged
dpbp.0                          plugged
dpcon.0                         plugged
-----
====================================================
Creating AIOP Tool Container
Assigned dpaiop.0 to dprc.3
Assigned dpmcp.28 to dprc.3
AIOP Tool Container dprc.3 created
----- Contents of AIOP Tool Container: dprc.3 -----
dprc.3 contains 2 objects:
object          label           plugged-state
dpaiop.0                        plugged
dpmcp.28                        plugged
-----
====================================================
Performing VFIO mapping for AIOP Tool Container (dprc.3)
Performing vfio mapping for dprc.3
========== Summary =================================
 AIOP Container: dprc.2
 AIOP Tool Container: dprc.3
====================================================
root@localhost:/mnt# find /usr/ -name aiop_reflector.elf
/usr/local/aiop/bin/LS1088A/aiop_reflector.elf
/usr/local/aiop/bin/LS2085A/aiop_reflector.elf
/usr/local/aiop/bin/LS2088A/aiop_reflector.elf
root@localhost:/mnt# aiop_tool load -g dprc.3 -f /usr/local/aiop/bin/LS1088A/aiop_reflector.elf &
[1] 4136
root@localhost:/mnt# [  522.876914] arm-smmu 5000000.iommu: Unhandled context fault: fsr=0x402, iova=0x        8182000077, fsynr=0x300010, cb=6
AIOP Image (/usr/local/aiop/bin/LS1088A/aiop_reflector.elf) with args ((null)) loaded successfully.

root@localhost:/mnt# cat /dev/fsl_aiop_console | grep REFLECTOR
REFLECTOR : Successfully configured ni0 (dpni.2) ""
REFLECTOR : dpni.2 <---connected---> dpmac.2 (MAC addr: 00:00:00:00:00:07)
REFLECTOR : Successfully configured ni1 (dpni.1) ""
REFLECTOR : dpni.1 <---connected---> dpmac.1 (MAC addr: 00:00:00:00:00:06)
REFLECTOR : NI 0 link is UP

When using a Packet Generator to inject traffic, connect one port of the packet generator to MAC1 of RDB-1 and a second port to MAC2 of RDB-1.

pastedImage_5.png

During frame processing, the AIOP Logger will print the following brief information about every reflected packet:

       NI ID on which the frame was processed

      AIOP Core number on which the task executes

      Received IP source and destination addresses

# tail –f /dev/fsl_aiop_console
RX on NI 0 | CORE:15
MAC_SA: 00-10-94-00-00-02 MAC_DA: 00-00-00-00-00-06
IP_SRC: 192.85.1.1 IP_DST: 192.0.0.1
RX on NI 0 | CORE:14
MAC_SA: 00-10-94-00-00-02 MAC_DA: 00-00-00-00-00-06
IP_SRC: 192.85.1.2 IP_DST: 192.0.0.1
. . .
RX on NI 0 | CORE:9
MAC_SA: 00-10-94-00-00-02 MAC_DA: 00-00-00-00-00-06
IP_SRC: 192.85.1.3 IP_DST: 192.0.0.1

Thanks,

Yiping

0 件の賞賛
返信