Real-TimeEdge SW Image Build fails because oe-runmake failed on do-compile phase.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Real-TimeEdge SW Image Build fails because oe-runmake failed on do-compile phase.

1,180件の閲覧回数
weilinja
Contributor I

Hi,

I am trying to build a Real-Time edge software image based on fsl-image-networking for my LS1028ARDB according to RTEDGEYOCTOUG_REV2.2.pdf chapter 8

In last step,when I use “bitbake fsl-image-networking” to build LS1028ARDB image, Igot those errors:

ERROR: binutils-cross-aarch64-2.36.1-r0 do_compile: oe_runmake failed
ERROR: binutils-cross-aarch64-2.36.1-r0 do_compile: Execution of '/home/forlinx/yocto-sdk/build_ls1028ardb/tmp/work/x86_64-linux/binutils-cross-aarch64/2.36.1-r0/temp/run.do_compile.3245' failed with exit code 1
ERROR: Logfile of failure stored in: /home/forlinx/yocto-sdk/build_ls1028ardb/tmp/work/x86_64-linux/binutils-cross-aarch64/2.36.1-r0/temp/log.do_compile.3245

and

ERROR: Task (/home/forlinx/yocto-sdk/sources/poky/meta/recipes-devtools/binutils/binutils-cross_2.36.bb:do_compile) failed with exit code '1'

What am I missing here?

Thank you for your kind help.

 

タグ(2)
0 件の賞賛
返信
0 返答(返信)