RCW queries based on LS1043ARDB-PD reference board

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

RCW queries based on LS1043ARDB-PD reference board

1,508 次查看
Abhilash_PV
Contributor I

Following are the queries on RCW based on the LS1043ARDB-PD reference board:

1. What is the value of C1_PLL_SEL in the RCW?

2. Is there any provision to set LVDD in the RCW similar to TVDD?

0 项奖励
回复
4 回复数

1,506 次查看
ufedor
NXP Employee
NXP Employee

1) RCW from the QorIQ LS1043A Reference Design Board Getting Started Guide:

00000000: 08100010 0a000000 00000000 00000000
00000010: 14550002 80004012 e0025000 c1002000
00000020: 00000000 00000000 00000000 00038800
00000030: 00000000 00001101 00000096 00000001

C1_PLL_SEL = 0b0000

2) No.

0 项奖励
回复

1,479 次查看
Akshayv
Contributor II

Hi, 

How does the processor know the voltage selected for LVDD. 

LVDD is similar in logic like TVDD.

where, TVDD voltage level is informed to the processor through RCW settings.

So, will the processor respond without any issues if we change the voltage on LVDD from 1.8 V to 2.5 V rather than informing the processor to expect for 2.5V in LVDD.

 

----

Thanks & Regards,

Akshay V 

0 项奖励
回复

1,483 次查看
Akshayv
Contributor II

Hi, 

Will the processor respond without any issues if we change the voltage on LVDD from 1.8 V to 2.5 V rather than informing the processor to expect for 2.5V in LVDD.

 

----

Thanks & Regards,

Akshay V 

0 项奖励
回复

1,472 次查看
ufedor
NXP Employee
NXP Employee

You wrote:

> Is there any provision to set LVDD in the RCW similar to TVDD?

The answer was: "No."

Because LVDD-powered I/Os differ from TVDD-powered I/Os.

0 项奖励
回复