Questions about USB3.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Questions about USB3.0

1,225件の閲覧回数
Victor97
Contributor I

Hi:

I use the cmds as follows to mount SSD as USB device,so i can transfer documentions from PC to my board.

However,when they are transfering files,if I pull out the USB cable,the USB module will die on my board.

I can't use 'rmmod' to remove the 'g_mass_storage' module,and the rmmod will also die in exiting.

How can i solve this probelm without rebooting?

2.png

1.png3.png

0 件の賞賛
返信
1 返信

1,202件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Configure Tree View Options Description
USB Gadget support --->
<M> USB Gadget functions configurable through configfs
       [*] Mass storage
<M> USB Gadget precomposed configurations
<M> Mass Storage Gadget

dts configuration

usb0: usb3@2f00000 {
          compatible = "snps,dwc3";
          reg = <0x0 0x2f00000 0x0 0x10000>;
          interrupts = <0 60 0x4>;
          dr_mode = "peripheral";
          snps,quirk-frame-length-adjustment = <0x20>;
          snps,dis_rxdet_inp3_quirk;
          maximum-speed = “super-speed”;
};

# dd if=/dev/zero of=./test bs=1M count=500
# insmod libcomposite.ko
# insmod usb_f_mass_storage.ko
# insmod g_mass_storage.ko file=test

Attach the USB cable between target board and Linux host machine
A new external hard drive appears on the host.  You may now use the host's tools to initialize and format the drive, and write data to it.  To avoid data loss or corruption, make sure to unmount the drive from the host to safely remove it when finished.   You can then unload the mass storage driver:

E.g;

root@xiao:~#fdisk /dev/sdc

root@xiao:~# mkfs.ext2 /dev/sdc1 

root@xiao:~# mount /dev/sdc1 /mnt

root@xiao:~# dd if=/dev/zero of=src_img bs=1M count=10

root@xiao:~#  cp src_img /mnt

 

0 件の賞賛
返信