on lx2160ardb-rev2 board, DDR is 16GB 2RX8 PC4-3200AA-EZZZ-11, but now we design a new board, use DDR 4GB 1RX16 PC4-2400T-UC0-11, boot message of UART1 is
NOTICE: UDIMM HMA851U6AFR6N-UH
ERROR: DDR clock (MCLK cycle 625 ps) is fater than DIMM can support.
ERROR: cas latency is too large 42
ERROR: Calculating DDR registers failed
ERROR: Calculate register error
so what DDR we can use ??
Thanks!
but 2400t DDR4 is slower than PC4-3200AA, what DDR4 can I use ?
this problem have been resolved.thanks
I need to faster DDR frequency, because 2400MT/S is slower than 3200MT/S.
or slower DDR DIMM to 2400MT/S.
maybe, I want more to know how can I change the DIMM to 2400MT/s ???
need to change RCW config ? or change the ATF code ??
what should I change ???
Thanks!
Your board is set to run DDR memory at 3200MT/s speed, however your memory module supports 2400MT/s speed maximum, this causes the error. So you need either to use faster UDIMM, or changes settings to slower DDR frequency.
Regards,
Bulat
Hi Bulat: thanks for your help.. I need to faster DDR frequency, because 2400MT/S is slower than 3200MT/S. or slower DDR DIMM to 2400MT/S. maybe, I want more to know how can I change the DIMM to 2400MT/s ??? need to change RCW config ? or change the ATF code ?? what should I change ??? Thanks!