Query on LX2160A SERDES Pin mapping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Query on LX2160A SERDES Pin mapping

1,185件の閲覧回数
Aathi1122000
Contributor I

We are using LX210A Processor in our design, We have connected different interfaces in the same SERDES : For Example:If we connect the PCIe on Lane 4,5, SGMII on Lane6 and SGMII on Lane 7 ,Is necessary to provide GNDS/NC in between the pins. Please suggest us the solution in detail.

0 件の賞賛
返信
1 返信

1,138件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

LX2160 has a fixed ball map and if there are GND or NC pins in between then use them. For not used interface, refer LX2160 design checklist for guidelines.

0 件の賞賛
返信