Query on LX2160A SERDES Pin mapping

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Query on LX2160A SERDES Pin mapping

1,195 Views
Aathi1122000
Contributor I

We are using LX210A Processor in our design, We have connected different interfaces in the same SERDES : For Example:If we connect the PCIe on Lane 4,5, SGMII on Lane6 and SGMII on Lane 7 ,Is necessary to provide GNDS/NC in between the pins. Please suggest us the solution in detail.

0 Kudos
Reply
1 Reply

1,148 Views
yipingwang
NXP TechSupport
NXP TechSupport

LX2160 has a fixed ball map and if there are GND or NC pins in between then use them. For not used interface, refer LX2160 design checklist for guidelines.

0 Kudos
Reply