Programming LS1046ARDB Ethernet with 32bit RTOS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Programming LS1046ARDB Ethernet with 32bit RTOS

跳至解决方案
1,775 次查看
srak
Contributor III

I'm trying to program Ethernet port (independent mode) for an RTOS. The RTOS I use is 32-bit. U-boot is used to load the RTOS.

For Ethernet program, I understand that I need to load FMAN microcode.  I guess, FMAN microcode can work with 32-bit access. But, when I check the LS1046A Reference manual, it says QMAN S/W Portal (05_0000_0000) is not supported for 32-bit access. Does FMAN microcode uses this QMAN S/W portal? Does this mean microcode/Ethernet port cannot be programmed with 32-bit RTOS?

Thanks in advance for any tips/information.

0 项奖励
回复
1 解答
1,738 次查看
yipingwang
NXP TechSupport
NXP TechSupport

FMan ucode and QMAN is independent to ARM operating system.

在原帖中查看解决方案

1 回复
1,739 次查看
yipingwang
NXP TechSupport
NXP TechSupport

FMan ucode and QMAN is independent to ARM operating system.