Programming LS1046ARDB Ethernet with 32bit RTOS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Programming LS1046ARDB Ethernet with 32bit RTOS

ソリューションへジャンプ
1,781件の閲覧回数
srak
Contributor III

I'm trying to program Ethernet port (independent mode) for an RTOS. The RTOS I use is 32-bit. U-boot is used to load the RTOS.

For Ethernet program, I understand that I need to load FMAN microcode.  I guess, FMAN microcode can work with 32-bit access. But, when I check the LS1046A Reference manual, it says QMAN S/W Portal (05_0000_0000) is not supported for 32-bit access. Does FMAN microcode uses this QMAN S/W portal? Does this mean microcode/Ethernet port cannot be programmed with 32-bit RTOS?

Thanks in advance for any tips/information.

0 件の賞賛
返信
1 解決策
1,744件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

FMan ucode and QMAN is independent to ARM operating system.

元の投稿で解決策を見る

1 返信
1,745件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

FMan ucode and QMAN is independent to ARM operating system.