Hi All,
I have a ls1043 based custom board and I am able to use my custom RCW and 2018.09 u-boot to boot just fine.
I am trying the u-boot text location on QSPI flash from 0x100000 to 0x10000.
Looks like that requires 2 changes, RCW/PBL and u-boot itself.
RCW change:
The RCW/PBL change to change the Boot location pointer high-order address (BOOTLOCPTRH) Page 457 of LS1043ARM.pdf
--- rcw/LSDK-18.12/mainline/src/ls1043aqds/RR_FQPP_1455/rcw_1600_qspiboot_T20.rcw 2019-09-27 22:11:49.000000000 -0700
+++ /rcw/LSDK-18.12/mainline/src/ls1043aqds/RR_FQPP_1455/rcw_1600_qspiboot.rcw 2019-09-27 22:11:49.000000000 -0700
@@ -147,7 +147,7 @@
 // QSPI flash clock
 write 0x57015c, 0x40100000
 write 0x570600, 0x00000000
-write 0x570604, 0x40100000
+write 0x570604, 0x40010000
 .end
patched for u-boot as below:
diff --git a/configs/ls1043aqds_qspi_defconfig b/configs/ls1043aqds_qspi_defconfig
index 2f14022..a4ad5a8 100644
--- a/configs/ls1043aqds_qspi_defconfig
+++ b/configs/ls1043aqds__qspi_defconfig
@@ -1,6 +1,6 @@
 CONFIG_ARM=y
 CONFIG_TARGET_LS1043AQDS=y
-CONFIG_SYS_TEXT_BASE=0x40100000
+CONFIG_SYS_TEXT_BASE=0x40010000
 CONFIG_FSL_LS_PPA=y
 CONFIG_DISTRO_DEFAULTS=y
 CONFIG_NR_DRAM_BANKS=2
No luck with these change.
After I flash the u-boot to the new location 0x10000 and reset, the unit never comes up.
Can someone please help advice if there is something else that needs to be done to relocate u-boot?
Thanks,
Bhanu
ls1043 ask
u-boot image
u-boot init
 
					
				
		
Hi ufedor,
> If "not" - which images were used when booting is possible?
Sorry, I did not catch that. Please find the known good images attached. I called then "GOLD".
2b094bd104c0fe61af5a4038e968d241eb836fc7 rcw_1600_qspiboot_T40.bin.swapped.GOLD
3a991dcd0b25da8995cbdf71e991d40d5c0f7406 u-boot_ls1043aqds_wg_t40_qspi.bin.GOLD
Thanks,
Mukund J
 ufedor
		
			ufedor
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Sorry for the delay.
I've inspected provided images and did not find any obvious issue.
Please enable debug messages in U-Boot and use CodeWarrior to determine the processor state during unsuccessful boot.
 
					
				
		
Hi,
The board does not have JTAG on board. Does u-boot support console stubs to just like KGDB?
Thanks
 ufedor
		
			ufedor
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Using debug messages it can be possible to determine position where the booting stops.
 
					
				
		
Hiufedor,
If you look into the screenlog log file(snippet below), a reset after programming "u-boot_ls1043aqds_wg_t40_qspi.bin.zip" and "rcw_1600_qspiboot_T40.bin.swapped.zip kills the boards and does not bring it up anymore.
Snippet from the screenlog:
=> cmp.b 0x82000000 0x80000000 0xe0
Total of 224 byte(s) were the same
=> reset
resetting ...
Does not BOOT after this.
1. And I cannot figure what in those files cause this failure.
2. And how to fix it so that when I relocate the uboot to qspi offset 0x10000, it works.
Mukund J
 ufedor
		
			ufedor
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		If "not" - which images were used when booting is possible?
 
					
				
		
Hi Ufedor,
Did you notice the attachments you were asking for?
Did you get a chance to review the?
Mukund J
 
					
				
		
I have attached more than screenlog.5.zip
I have attached these 4 files, RCW and u-boot part of those atttachments. Do you see them?
files I have attached:
screenlog.5.zip
rcw_1600_qspiboot_T40.rcw.zip
u-boot_ls1043aqds_wg_t40_qspi.bin.zip
rcw_1600_qspiboot_T40.bin.swapped.zip
Thanks,
Mukund J
 ufedor
		
			ufedor
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Are you saying that the "screenlog.5.zip" was obtained when the "u-boot_ls1043aqds_wg_t40_qspi.bin.zip" and "rcw_1600_qspiboot_T40.bin.swapped.zip" were programmed into the SPI Flash?
If "not" - which images were used when booting is possible?
 
					
				
		
Hi ufedor,
I did not quite get your question. But, I will try and answer a few things.
The images I used are attached. And these are the once that fail.
And these have the patch I provided early on applied to them.
u-boot_ls1043aqds_wg_t40_qspi.bin.zip
rcw_1600_qspiboot_T40.bin.swapped.zip
Both u-boot and RCW are from LSDK18.12.
u-boot/2018.09
rcw/LSDK-18.12
Does it answer your question? Otherwise, can you make it little more clear on what you are asking.
Thanks,
Mukund J
 ufedor
		
			ufedor
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		You provided "screenlog.5" log.
Which RCW and U-Boot images correspond to this log?
 
					
				
		
Hi ufedor,
Thanks for looking into this.
I am doing standalone builds for RCW and u-boot as I am building outside of yocto in my own build environment.
So, I don't have the composite build. Is there a quick way to make one out of yocto build.
I have also attached a bootlog, so that might help.
my instructions to install the image are below:
#How to upgrade rcw
tftp 0x82000000 rcw-tweeks/t40/mj-tweeked/rcw_1600_qspiboot_T40.bin.swapped
sf probe 0:0;sf erase 0 +$filesize;sf write 0x82000000 0 $filesize
# How to upgrade u-boot
tftp 82000000 rcw-tweeks/t40/mj-tweeked/u-boot_ls1043aqds_wg_t40_qspi.bin
sf probe 0:0;sf erase 10000 +$filesize;sf write 82000000 10000 $filesize
Mukund J
 ufedor
		
			ufedor
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Which RCW and U-Boot images are used when the processor is capable to boot?
 ufedor
		
			ufedor
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Described steps are correct.
Please ensure that binary images of RCW and U-Boot were programmed to the SPI Flash correctly.
Please consider that LSDK is capable to build composite firmware image (pre-built images are provided at LSDK Open Source , LSDK IMAGES) - refer to the LSDK Documentation:
Please provide the resulting composite firmware image for inspection.