Power on Sequence for LS2088A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Power on Sequence for LS2088A

1,157件の閲覧回数
sekuru_saimukhe
Contributor I

Hi,

I am using LS2088A in a project.

Below is the power on sequencing which I am implementing in my circuit. 

Initially all the IO and PLL power rails (3.3V, 1.8V, 1.35V, 1V_SVDD, 1V_USBSVDD) are released.

After all these power rails are released then the 1V05 core voltage is released and then the 1V2 DDR supply voltage is released.

Please let me know whether this sequence is fine or any correction is required.

0 件の賞賛
返信
1 返信

1,115件の閲覧回数
ufedor
NXP Employee
NXP Employee

Described sequence is in accordance with the QorIQ LS2088A/LS2048A Data Sheet, 3.2 Power sequencing assuming that:

1) VDD is at 90% of its value before GnVDD reaches 10% of its value

2) All supply voltages are stable within 400 ms.

0 件の賞賛
返信