PPS signal based on PTP Hardware Clock for LS1028A-RDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PPS signal based on PTP Hardware Clock for LS1028A-RDB

Jump to solution
2,692 Views
ceroone
Contributor II

Hello,

According to this post (https://community.nxp.com/t5/Other-NXP-Products/PPS-signal-on-LS1021A-TSN/m-p/1296948#M11360), it is possible to generate a PPS signal from the PTP Hardware Clock on the LS1028A-RDB.

Could you please provide me with a link that explains the steps to follow to do this, or at least some additional information?

What about the IMX8MPEVK? Is the PPS signal generation supported on this board too? Is the procedure similar?

Thank you in advance.

ceroone

0 Kudos
Reply
1 Solution
2,686 Views
r8070z
NXP Employee
NXP Employee

There is a link to the OpenIL user manual in the post you mentioned, which says the LS1028A-RDB supports the PPS signal, but does not say the same for the IMX8MPEVK. It also provides commands to use and test PPS generation under OpenIL. The corresponding commands in case of using the Layerscape Software Development Kit on LS1028A can be found in the LSDK user manual.
 https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-F53B3CE9-AB67-4713-9...
https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-F53B3CE9-AB67-4713-9...
The low-level programming model of the LS1028A IEEE 1588 module can be found in Section 16.3 Ethernet Controller (ENETC) of the QorIQ LS1028A Reference Manual. You can download it from the LS1028A web page
https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/la...

View solution in original post

0 Kudos
Reply
1 Reply
2,687 Views
r8070z
NXP Employee
NXP Employee

There is a link to the OpenIL user manual in the post you mentioned, which says the LS1028A-RDB supports the PPS signal, but does not say the same for the IMX8MPEVK. It also provides commands to use and test PPS generation under OpenIL. The corresponding commands in case of using the Layerscape Software Development Kit on LS1028A can be found in the LSDK user manual.
 https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-F53B3CE9-AB67-4713-9...
https://docs.nxp.com/bundle/GUID-3FFCCD77-5220-414D-8664-09E6FB1B02C6/page/GUID-F53B3CE9-AB67-4713-9...
The low-level programming model of the LS1028A IEEE 1588 module can be found in Section 16.3 Ethernet Controller (ENETC) of the QorIQ LS1028A Reference Manual. You can download it from the LS1028A web page
https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/la...

0 Kudos
Reply