Loading LS1043ARDB's u-boot image using qemu-system-aarch64

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Loading LS1043ARDB's u-boot image using qemu-system-aarch64

1,615 次查看
ts1234
Contributor III

How do I load the LS1043ARDB's u-boot.bin image on qemu-system-aarch64?

It is working only for the linux kernel and rootfs, but it does not load the u-boot.bin (screen hang..no logs).

I have tried uboot from LSDK as well as from OpenIL.

I have also checked these uboot images with the latest qemu (5.2) release as well.

0 项奖励
回复
1 回复

1,604 次查看
bpe
NXP Employee
NXP Employee


u-Boot expects to run on a real hardware. Although in theory it is possible to
run it in a VM, such scenario is outside of the supported feature set in either
LSDK or OpenIL.

 

Best Regards,
Platon

 

0 项奖励
回复