Loading LS1043ARDB's u-boot image using qemu-system-aarch64

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Loading LS1043ARDB's u-boot image using qemu-system-aarch64

1,624 Views
ts1234
Contributor III

How do I load the LS1043ARDB's u-boot.bin image on qemu-system-aarch64?

It is working only for the linux kernel and rootfs, but it does not load the u-boot.bin (screen hang..no logs).

I have tried uboot from LSDK as well as from OpenIL.

I have also checked these uboot images with the latest qemu (5.2) release as well.

0 Kudos
Reply
1 Reply

1,613 Views
bpe
NXP Employee
NXP Employee


u-Boot expects to run on a real hardware. Although in theory it is possible to
run it in a VM, such scenario is outside of the supported feature set in either
LSDK or OpenIL.

 

Best Regards,
Platon

 

0 Kudos
Reply