Load (for booting) the bl2.pbl and fip.bin file via CodeWarrior + JTAG TAP on LS1043ARDB?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Load (for booting) the bl2.pbl and fip.bin file via CodeWarrior + JTAG TAP on LS1043ARDB?

981 次查看
ts1234
Contributor III

How do I load (for booting) the bl2.pbl (RCW+PBI+BL2) and fip.bin file via CodeWarrior + JTAG TAP on LS1043ARDB?

Do I need to make any changes in the source code (rcw, pbl and uboot) to support the loading via JTAG?

0 项奖励
回复
1 回复

970 次查看
yipingwang
NXP TechSupport
NXP TechSupport

After installing CodeWarrior, please refer to section "7.7 Using flash programmer from eclipse IDE" in C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\Help\PDF\ARMv8_Targeting_Manual.pdf to do flash programming with CodeWarrior IDE.

Please program bl2.pbl  at 0x60000000 and fip.bin at 0x60100000.

You could refer to section 1 in 

https://community.nxp.com/t5/CodeWarrior-for-QorIQ-Knowledge/Use-CodeWarrior-for-ARMv8-to-Debug-U-bo...

0 项奖励
回复