Layerscape and MicroSD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Layerscape and MicroSD

4,779件の閲覧回数
miha_at_work
Contributor III

Hello.

I had made custom PCB with LS2084. When I did it I used LS2088ARDB-PA-DF schematic diagram as a reference. I have a question about level translators for SD card. As I see U205 and U206 (TXBN0304RSVR) and ST6G3244MEBJR is used instead. Will SD card work if I will use TXBN0304RSVR (or TXS02612)? I can't use ST6G3244MEBJR because it have too little BGA pitch. We will use SD card as boot device.

0 件の賞賛
返信
7 返答(返信)

4,669件の閲覧回数
Pavel
NXP Employee
NXP Employee

Use SD card or MicroSD card as boot device.

Interface of MicroSD is the same as SD card.

Have a great day,
Pavel Chubakov

4,669件の閲覧回数
Pavel
NXP Employee
NXP Employee

See schematic from the LS1043ARDB-PC Design Files (REV PC ):

https://www.nxp.com/webapp/Download?colCode=LS1043ARDB-PC&appType=license

Have a great day,
Pavel Chubakov

4,669件の閲覧回数
miha_at_work
Contributor III

Can I use MicroSD as a boot device? Or is SD card desired?

0 件の賞賛
返信

4,670件の閲覧回数
miha_at_work
Contributor III

Thank you.

0 件の賞賛
返信

4,669件の閲覧回数
Pavel
NXP Employee
NXP Employee

The TXBN0304RSVR is used as level translator for SDHC signals on the LS1043ARDB board. See the LS1043ARDB schematic:

https://www.nxp.com/downloads/en/printed-circuit-boards/LS1043ARDB_PD-39019-DF.zip

 

It means that the TXBN0304RSVR on your board also.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,669件の閲覧回数
miha_at_work
Contributor III

I had look at the LS1043ARDB schematic and it's BOM and I found there no any TXBN0304RSVR. On page 15 of document SPF-39019_F.pdf SDHC signals are connected to SD/MMC connector (5911M5001-LF) directly.

0 件の賞賛
返信

4,669件の閲覧回数
miha_at_work
Contributor III

*As I see U205 and U206 (TXBN0304RSVR) are not populated and ST6G3244MEBJR is used instead.

0 件の賞賛
返信