Layerscape LS1043A Footprint

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Layerscape LS1043A Footprint

2,422 Views
Wisteria
Contributor I

Dears,

In the datasheet of Layerscape LS1043A  page 255, the pitch of horizontal rows and vertical are the same 0.8mm (As shown in the figure 1). However, in the layerscape LS1043A reference design board , the pitch in the middle between two rwos is 1.6mm (As shwon in the figure 2). Is it a mistake ?

Thank you for your time and consideration.

Best Regards.

@Bulat 

0 Kudos
Reply
1 Reply

2,404 Views
Teddy1
Contributor II

Look at gerber file PSM.art or PSP.art for component place , pitch is 0.8mm.

 

0 Kudos
Reply