Layerscape LS1043A Footprint

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Layerscape LS1043A Footprint

2,420件の閲覧回数
Wisteria
Contributor I

Dears,

In the datasheet of Layerscape LS1043A  page 255, the pitch of horizontal rows and vertical are the same 0.8mm (As shown in the figure 1). However, in the layerscape LS1043A reference design board , the pitch in the middle between two rwos is 1.6mm (As shwon in the figure 2). Is it a mistake ?

Thank you for your time and consideration.

Best Regards.

@Bulat 

0 件の賞賛
返信
1 返信

2,402件の閲覧回数
Teddy1
Contributor II

Look at gerber file PSM.art or PSP.art for component place , pitch is 0.8mm.

 

0 件の賞賛
返信