Latest kernel support for LS1021atwr

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Latest kernel support for LS1021atwr

2,034件の閲覧回数
jackou
Contributor I

Hi,

I am working on LS1021atwr board, with yocto rocko release, the kernel version is 4.9.  

I check from yocto recipe list, for linux qoriq kernel, the latest is gatesgarth (5.4.3) or master (5.4.47).   Does it mean these are the latest support for LS1021atwr ?

If yes, any plan to move to newer kernel versions ? 

Thanks a lot ! 

0 件の賞賛
返信
3 返答(返信)

1,950件の閲覧回数
jackou
Contributor I

Hi Pavel,

I tried the yocto link above and checked out gatesgarth branch.

It is using kernel 5.10.9.  

Is this version stable enough for ls1021atwr ?

Thanks a lot !

0 件の賞賛
返信

2,018件の閲覧回数
Pavel
NXP Employee
NXP Employee

NXP offers LSDK2012 for the TWR-LS1012a board. See the following document:

https://www.nxp.com/docs/en/user-guide/LSDKUG_Rev20.12.pdf

 

This LSDK supports kernel version 4.19.139 and 5.4.47.

 

NXP offers also SDK 2.7 yocto BSP for the TWR-LS1021a:

https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/about/

 

This BSP supports gatesgarth (5.4.3).

0 件の賞賛
返信

1,949件の閲覧回数
jackou
Contributor I

Hi Pavel,

I tried the yocto link above and checked out gatesgarth branch.

It is using kernel 5.10.9.  

Is this version stable enough for ls1021atwr ?

Thanks a lot !

タグ(1)
0 件の賞賛
返信