Latest Available Kernel for LS1043A

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Latest Available Kernel for LS1043A

1,892件の閲覧回数
sandeepajesh
Contributor III

Hi Guys,

We are working on a LS1043A based board and we want to use latest supported kernel.

Can someone please help me with this. From where I can get latest kernel for LS1043A.

Regards

SS

ラベル(1)
1 返信

1,724件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello sandeep sharma,

The latest SDK release for LS1043 is SDK 2.0 1703, you could download ISOs from Linux® SDK for QorIQ ® Processors|NXP.

According to SDK 1703 linux package recipe, the git tree address is as the following.

git://git.freescale.com/ppc/sdk/linux.git

1ae843c08261402b2c35d83422e4fa1e313611f4


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------