LX2160A boot loader location

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LX2160A boot loader location

跳至解决方案
2,981 次查看
dmitri_lechtchinski
Contributor III

Hello,

Which devices can be used for loading boot loader image from on SoC startup? (XSPI, ...?)

Can an image be loaded from NVMe device?

Thanks,
Dmitri

0 项奖励
回复
1 解答
2,975 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LX2160A Reference Manual, Table 13. RCW Source and Flash Mode Encodings.

> Can an image be loaded from NVMe device?

No.

在原帖中查看解决方案

1 回复
2,976 次查看
ufedor
NXP Employee
NXP Employee

Please refer to the QorIQ LX2160A Reference Manual, Table 13. RCW Source and Flash Mode Encodings.

> Can an image be loaded from NVMe device?

No.